{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What Equipment settings do I need in Vijeo Designer for my Harmony/Magelis HMI to communicate to a Modicon M340 or M580 PLC via Modbus Serial or Modbus TCP/IP?

Article available in these languages: Spanish

Issue

The M340 and M580 Modbus Serial and Modbus TCP/IP protocols require particular settings in Vijeo Designer in order for a Harmony/Magelis HMI to communicate to them via IEC61131 Syntax.

Product Line
Modicon M340 PLC, Modicon M580 PLC, Harmony/Magelis HMI (all series), Vijeo Designer (all versions)

Environment
Modbus protocol setup in Vijeo Designer

Resolution

To access the Modbus Equipment Node for Modbus TCP/IP, double-click on the IO Manager -> ModbusTCPIP01 -> ModbusEquipment0x node.

Likewise, for Modbus RTU (Serial), double-click on the IO Manager -> ModbusRTU0x-> ModbusEquipment0x node.

In this window, confirm the following 3 settings:

  1. Tick the IEC61131 Syntax checkbox (this uses %M, %MW addressing instead of “00001, 40001” addressing)
  2. Select Addressing Mode = 0-based (Default) – The M580 starts at %MW0 (unlike some older PLCs that start at %MW1).
  3. Choose Double Word word order = Low word first

Schneider Electric Global

Attachment(s)
Modbus RTU settings.png [67.61 KB]
Modbus TCP settings.png [261.34 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: