undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
In SoMove why is the fast scope type not available when working with an ATV12?
Issue:
Why in the ATV12 is the fast scope type not available when working with SoMove?

Product Line:
Altivar 12

Environment:
SoMove commissioning software

Cause:
Fast scope selection is grayed out, not selectable

Resolution:
ATV12 is a basic drive and does not have Fast Scope function implemented.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: