Issue:
Availability of Dual ramps with the ATV320 drives.
Product Line:
ATV320
Environment:
All serial numbers
Cause:
Application requirement
Resolution:
Yes, There is a second acceleration ramp option, ACC2 (ranges from 0.00 - 6,000 seconds)

Availability of Dual ramps with the ATV320 drives.
Product Line:
ATV320
Environment:
All serial numbers
Cause:
Application requirement
Resolution:
Yes, There is a second acceleration ramp option, ACC2 (ranges from 0.00 - 6,000 seconds)
Released for:Schneider Electric Global