undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
EcoStruxure Machine Expert system requirements for PC
Issue
What are the hardware and software requirements for my PC to be able to install and run EcoStruxure Machine Expert PLC configuration software?

Product Line
EcoStruxure Machine Expert v1.2
EcoStruxure Machine Expert v2.0

Environment
PLC configuration software for Windows PC

Resolution
Hardware Requirements:

Minimum:
Processor: Intel® CoreTM 2 Duo (or later)
RAM: 4 GB
Free hard drive space: 8GB including the memory space for compact software installation, temporary space for execution and space for saving applications
Display: resolution 1280x1024 pixels
Peripherals: mouse or compatible pointing device, USB Type-A port
Web access: Web installation and registration requires Internet access to the system.

Recommended:
Processor: Intel® CoreTM i7 (or equivalent)
RAM: 8 GB
Free hard drive space: 15 GB for the full software installation, temporary space for execution and space for saving applications
Display: resolution 1920x1080 pixels
Peripherals: mouse or compatible pointing device, USB Type-A port
Web access: Web installation and registration requires Internet access to the system.


Software Requirements:
Thee EcoStruxure Machine Expert software supports the following operating systems:
Microsoft Windows® 7 SP1 Professional Edition 32 bits
Microsoft Windows® 7 SP1 Professional Edition 64 bits
Microsoft Windows® 8.1 Professional Edition 32 bits
Microsoft Windows® 8.1 Professional Edition 64 bits
Microsoft Windows® 10 Professional Edition 32 bits
Microsoft Windows® 10 Professional Edition 64 bits

And requires:
Microsoft .NET Framework 3.5 SP1
Microsoft .NET Framework 4.7.2 or 4.8

EcoStruxure Machine Expert literature contains PDF-formatted documents that require the installation of the Adobe Reader TM. This reader is not part of the EcoStruxure Machine Expert installation but can be downloaded from http://www.adobe.com/go/getreader

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: