Issue:
Running multiple instances of EcoStruxure Control Expert Simulator at the same time.
Product Line:
EcoStruxure Control Expert
Resolution:
As of EcoStruxure Control Expert V15.0, you can now simulate multiple instances of Control Expert programs. To simulate you would use a different port number for each instance. To do so, select PLC from the main menu and select "set address"
In the Simulator section, the Simulator's IP address is normally 127.0.0.1. Simply add a colon then the port number as shown.
In this example you can see the project connected to the simulator at port 504. For the other instance just change the port number to something other than 504. The other instance below is using port 503
Here you can see both of the Control Expert Simulators running simultaneously
Released for:Schneider Electric Global