undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to use the TRB142 Teltonika modem with the Modicon M221 Controller in EcoStruxure Machine Expert - Basic?
  1. Modem – RS232 configuration
First of all, it is strongly recommended to go to Teltonika website and retrieve the latest FW version of the TRB142 Teltonika.
https://wiki.teltonika-networks.com/view/TRB142_Firmware_Downloads

Connect the TRB142 modem to your PC thanks to the USB cable supplied with the modem.
Use the Quick Start Guide available with the modem TRB142 to change configuration of modem.
https://teltonika-networks.com/products/gateways/trb142

To enter the gateway's Web interface, type http://192.168.2.1 into the URL field of your Internet browser.

Use this Login information:
  • Username: admin
  • Password: admin01

Go to Services >> Serial Utilities >> Modem Control:

Teltonika_newFW

From this page, Add a New Instance with the same communication settings as defined in the controller application:

Teltonika_newFW_2_M221
=> Click “Save & Apply

Note: Mode has to be set on Full Control. In this mode, the TRB142 modem is completely started when the 2G,3G,4G LEDs are blinking and all signal LEDs are OFF.

  1. M221 Controller – Serial Port and ASCII Manager configuration
Serial port configuration:

M221-SerialPortConfig

ASCII Manager configuration:

M221-ASCIIManagerConfig

Select Generic Modem and add the following init command:
AT&F; E0;S0=2; S3=13;S4=10;Q0;V1;+CBST=0,0,1;&W;+CMGF=0;+CNMI=2,2,0,0,0

NOTE: Refer to EcoStruxure Machine Expert - Basic online help for SMS configuration.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: