Circuit breaker innovations key to transforming data centre, industrial and commercial infrastructure efficiency and sustainability
South Africa
18/11/2025
By Kamogelo Makwana, Power Products Offer Manager at Schneider Electric
18 November 2025
Recent advancements in circuit breaker technology have seen a major step forward in setting new standards for efficiency and sustainability in data centres, industrial and commercial infrastructure.
When considering power efficiency challenges in such environments, several critical issues emerge. These environments typically experience high energy demand, driven not only by the operational requirements of running servers and equipment, but also by the intensive cooling systems needed to maintain optimal performance, especially in data centres.
Many of the inefficiencies stem from this dual energy burden: sustaining uninterrupted operations while managing temperature control effectively. In addition, there's a growing imperative to integrate renewable energy sources into their ecosystems to mitigate environmental impact and reduce reliance on conventional power grids.
South Africa faces many of the same power efficiency challenges seen globally across data centres and industrial or commercial infrastructure. Escalating energy demands remain a central concern, particularly in data centres, where continuous operation and high-performance cooling systems drive substantial consumption.
Lack of energy reliability
While load shedding has eased in recent months, the availability of stable grid power remains inconsistent, making energy reliability a persistent hurdle. In this context, facilities are also grappling with the need to adopt emerging technologies that optimise energy usage and enable seamless integration of renewable sources.
Addressing these interconnected challenges is essential for improving overall energy efficiency, enhancing sustainability and supporting long-term resilience across infrastructure sectors.
Innovations in low-voltage circuit breakers not only enhance operational continuity but also support sustainability goals by minimising waste and promoting effective energy management practices. Furthermore, improved safety features protect maintenance personnel while ensuring reliable power distribution.
For example, the emergence of smart technologies in electrical distribution, particularly Internet of Things (IoT) -enabled circuit breakers, has redefined the way facilities manage power efficiency and operational reliability.
This is because real-time monitoring empowers facilities to respond swiftly to dynamic electrical conditions. This capability is no longer a luxury but a necessity, enabling operators and end-users to make informed, real-time decisions that directly impact energy efficiency and system uptime.
Remote monitoring and control
IoT-enabled circuit breakers allow for remote monitoring and control, reducing the need for physical presence. When excessive power consumption is detected, maintenance personnel can be deployed immediately, minimising downtime and preventing cascading failures.
At the same time, real-time analytics, powered by Artificial Intelligence (AI) within power monitoring software associated to the equipment, help with diagnosing potential equipment failures, pin-pointing root causes behind power anomalies and energy wastage, and operational inefficiencies.
Remote monitoring and control capabilities offered IoT enable breakers overall offer significant advantages in relation to operation efficiency, reliability, cost efficiency and most importantly, safety to personnel.
Personnel safety in electrical installations and operations remains one of the most crucial points in data centres and large-scale infrastructure. Remote control offers reduced exposure of personnel to arc flash risks, which account to an estimated 80% of personnel fatalities in electrical installations.
The most valuable and expensive asset for any company is personnel, aside from the financial and operational implications, the cost of human life cannot be calculated, and this would also come with legal and reputational implications to the any of the employers in the data centre, industrial and commercial infrastructure. Beyond equipment, these technologies play a vital role in safeguarding personnel.
Transformative shift
In the realm of power distribution, the integration of IoT-enabled circuit breakers, such as those in Schneider Electric’s MTZ Active range, ushers in a transformative shift. These devices bring intelligence and connectivity to critical infrastructure, fundamentally changing how efficiency, maintenance and sustainability are managed.
Ultimately, emerging technologies like real-time data access and predictive maintenance capabilities are significantly reshaping energy management. IoT-enabled breakers allow end users to gain access to real-time data that drives fact-based decision-making, enabling facilities to operate at peak efficiency, prevent unnecessary energy use, protect both equipment and personnel, and support carbon reduction goals.
This minimises inefficiencies, reduces excessive energy consumption and ensures operations run with minimal disruption.
End
About Schneider Electric
Schneider’s purpose is to create Impact by empowering all to make the most of our energy and resources, bridging progress and sustainability for all. At Schneider, we call this Life Is On.
Our mission is to be the trusted partner in Sustainability and Efficiency.
We are a global industrial technology leader bringing world-leading expertise in electrification, automation and digitization to smart industries, resilient infrastructure, future-proof data centers, intelligent buildings, and intuitive homes. Anchored by our deep domain expertise, we provide integrated end-to-end lifecycle AI enabled Industrial IoT solutions with connected products, automation, software and services, delivering digital twins to enable profitable growth for our customers.
We are a people company with an ecosystem of 150,000 colleagues and more than a million partners operating in over 100 countries to ensure proximity to our customers and stakeholders. We embrace diversity and inclusion in everything we do, guided by our meaningful purpose of a sustainable future for all.
Attached files
press_release_template_june_2024_r (1) (2) (AutoRecovered).pdf
PDF, document01/12/2025View asset
Contact press

Schneider Electric Anglophone Africa Media Relations
0112546000 africa.pr@se.com
Adoption of Wiztrust's Blockchain Certification Platform
From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.