No one should be left behind – why utilities must prioritise maintenance of SA’s remote data centres
South Africa
03/06/2025
By Ben Selier, Vice President, Secure Power for Anglophone Africa at Schneider Electric
03 June 2025,
The story of power generation is more than meets the eye. Beyond energy distribution and the infrastructure that enable it, are the IT systems that play a fundamental role in keeping systems running. However, it is also these invisible, if you will, Point of Presence (PoP) data centres – located the remotest parts of our country – that often go unseen.
The reality is that in order for utilities to deliver safe, reliable and sustainable electricity to even the smallest of South African towns, the remote sites must be maintained and secured. You cannot separate the infrastructure that manages input from the systems that enable output.
Data centres today serve the digital infrastructure of utilities; whether it is ensuring billing accuracy or controlling grid distribution, these facilities provide essential IT services that enable the services to function properly.
Like physical operational infrastructure, IT failure can also lead to service interruption, safety risks, and increased operational costs. And unfortunately, particularly at remote sites, the maintenance of IT systems isn’t always prioritised.
It becomes a bit contradictory when a transformer can still deliver electricity, but the utility’s billing or monitoring system is offline due to battery failure or overheating.
Indeed, acid leaks, non-functional air condition and unstable UPS systems can be downright catastrophic. If left unchecked, these remote sites can experience complete system outages which are not costly but time consuming to repair due to the isolated location of some of these sites.
There are solutions, today
So, what can be done to provide some relief to our country’s already overburdened utilities? Data Centre Infrastructure Managements (DCIM) overcomes a lot of the abovementioned challenges.
DCIM offerings which today incorporate Building Management Systems (BMS) and facility management platforms offer importantly functionality such as early warnings through the use environmental sensors, helping utilities act before minor issues escalate.
Also, vibration sensors can detect irregularities in generators long before it fails, and temperatures spikes in battery rooms can prompt immediate cooling interventions, avoiding the need for expensive replacements.
Importantly, DCIM overcomes the need to travel hundreds of kilometres to physically inspect every POP data centre which is extremely challenging given the size and spread of South Africa’s grid infrastructure. DCIM’s centralised monitoring systems allow utilities to keep tabs on all their sites from a single control room, often located hundreds of kilometres away.
Schneider Electric’s DCIM offering is an integrated solution tailored to the needs of remote utility sites. It includes features like;
- Environmental and equipment monitoring of temperature, humidity, power load, UPS health, and more.
- Access control and surveillance - cameras installed both on site and inside racks for physical security.
- Vibration sensors – monitoring generators and other critical machinery.
- Centralised control and visibility that enable real-time insight from a single command centre.
- Proactive alerts which allow for early intervention before equipment fails.
The benefits are also immediate, reduced downtime, lower maintenance costs, improved safety, and longer equipment life cycles which, in turn, avoid large-scale repairs or replacement – all contributing to reduced capital expenditure.
END
About Schneider Electric
Our mission is to be the trusted partner in Sustainability and Efficiency.
We are a global industrial technology leader bringing world-leading expertise in electrification, automation and digitization to smart industries, resilient infrastructure, future-proof data centers, intelligent buildings, and intuitive homes. Anchored by our deep domain expertise, we provide integrated end-to-end lifecycle AI enabled Industrial IoT solutions with connected products, automation, software, and services, delivering digital twins to enable profitable growth for our customers.
We are a people company with an ecosystem of 150,000 colleagues and more than a million partners operating in over 100 countries to ensure proximity to our customers and stakeholders. We embrace diversity and inclusion in everything we do, guided by our meaningful purpose of a sustainable future for all.
Attached files
press_release_template_june_2024_r (1).pdf
PDF, document04/06/2025View asset
Contact press

Schneider Electric Anglophone Africa Media Relations
0112546000 africa.pr@se.com
Adoption of Wiztrust's Blockchain Certification Platform
From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.