Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

A rock solid case for circuit breaker diagnostics

By Casper Du Plessis, Power Systems Operational Manager: Services at Schneider Electric

24 August 2023

Circuit breakers are undoubtedly one of the unsung heroes of the electrical world.  It performs vitally important tasks: protecting an electrical circuit from damage caused by overcurrent/overload of short circuit.  In short, it interrupts current flow as soon as the protective relays detect a fault.

The above alone makes a solid case for why the circuit breakers require maintenance and, importantly, diagnostics. However, to place it in everyday context, it’s important that we take one step back and look at some of consequences of faulty breakers.

Foremost, when circuit breakers start to break in a plant or factory, it can lead to various problems, primarily downtime.

Moreover, if there are no spare parts available, the situation can be even more problematic. Replacing a breaker, especially an older one, is a time-consuming task that involves changing several connections, resulting in significant downtime.

This downtime doesn't just affect the faulty breaker; it can have a cascading effect on other systems, causing additional failures and disruptions.  In the current energy provision landscape, extended downtime should be avoided at all costs.

Fortunately, there are a number of expert service providers that offer both the entrenched auditing experience and diagnostics tools that ensure crucial components like circuit breakers are managed and maintained.

In fact, diagnostics are emerging as a critical success factor in improving electrical room safety, durability, and performance. Proper electrical equipment diagnostics requires a high level of human experience and expertise, sophisticated software tools, and broad access to equipment field performance data.

The question is what should you look for when choosing the right diagnostic offering?  Breaker diagnostic tools assess the speed of particular breakers over time, and whether it has slowed down, highlighting which ones should be repaired or replaced outright.

These diagnostic tools also provide detailed information and recommendations that will allow organisations to plan for the future.  It can determine how long a breaker can still be used and offer scenarios that outline what parts will still be available in the next ten years. 

It also generates reports that include data from visual inspections, as well as technical data from the various tests conducted on the breaker to assess its condition.

At Schneider Electric, our ProDiag diagnostic tools offer a combination of dedicated sensors and internal software that allow services personnel use to analyse trip units, relays, breakers, fuses, and other electrical components.

Our ProDiag Breaker tool identifies the symptoms of undetected incidents or degradation of equipment and offers the following additional benefits:

  • Detects the early stages of breaker degradation which isn’t necessarily detected during regular preventive maintenance.
  • Assists with protection of downstream electrical distribution equipment, goods, and the people operating them.
  • Enhances reliability, mitigating unexpected shutdown risks and operating costs.
  • Extends equipment lifespan, optimising TCO.

Attached files

  • A rock solid case for circuit breaker diagnostics.pdf

    PDF, document
    24/08/2023
    View asset

Contact press

Adoption of Wiztrust's Blockchain Certification Platform

Share this page:

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and contact centre
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
  • Terms and Conditions
  • Privacy Policy
  • Cookie Notice
  • Change your cookies settings