Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Lexium 28 be controlled via Modbus RS485
Full Modbus control of LXM28 is not possible because Modbus control words have not be included in the design.

However, it is possible to read and write parameters via Modbus, but it is not possible to control the drive via the Modbus channel because there are no
Modbus objects available on LXM28 for the "ControlWord" and also not available for the "ModesOfOperation"

It is possible to create some simple motion using Modbus because it is possible to write via Modbus and force the digital inputs on and off, this is covered in another FAQ.

Customers looking to control LXM28 via Magelis will need to choose a model that supports integrated CANopen master, (such as XBTGC or SCU) to control LXM28 via Magelis.

Magelis such as XBTGC and SCU are implemented into SoMachine and therefore the LXM28-PLCopen Library can be used.



Schneider Electric South Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and contact centre
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
  • Terms and Conditions
  • Privacy Policy
  • Cookie Notice
  • Change your cookies settings