Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the D-Line contactors rated to break DC voltages?
Issue:
Can the TeSys D line be used to control DC loads?

Product Line:
Tesys D contactors

Environment:
Products sold and used in the United States

Cause:
DC power circuit

Resolution:

Yes, 75 VDC (125 VDC for D115 & D150) per pole which means that through a four pole device breaking 300 VDC is possible by wiring all four power poles in series. However, be aware that the device current ratings will differ according to the number of poles in series and the type of application.

Devices are suitable but not UL Listed for DC applications.

More information on their DC ratings can be found in the current TeSys Motor Control and Protection Compentns catalog: https://www.se.com/us/en/download/document/MKTED210011EN/


Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings