Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the cradle rejection (cell keying) kits for NT/NW circuit breakers?
Issue:
What are the cradle rejection (cell keying) kits for NT/NW circuit breakers?

Product Line:
Circuit Breakers

Resolution:
Cell keying kits are standard, however the field installable kits are S33767 for NT, NWCELLKEY for NW.

NW cell keying history:
Cell keying kit for W/Y-frame (pins of varying lengths)  All production after December 2012: NWCELLKEY

Older part numbers:
S48562C was developed to provide complete mismatch protection. It is used on breakers and boards assembled in Columbia. This has been replaced with NWCELLKEY.
The S48562 kit has pins all the same length and is from France. It has gaps in protection against mismatch. It was sold to OEMs.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings