Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for the Kirk Key Interlocks for Powerpact and Masterpact breakers that customers can order direct from Kirk?
Product Line:
PowerPact M, P and R frame and Masterpact NT and NW Breakers

Resolution:
The following are the Kirk part numbers for PowerPact and Masterpact breakers that can be ordered from Kirk if the breaker has provisions for a Kirk lock installed. If the Powerpact breaker was not ordered with the provision factory installed, the breaker or accessory cover may be returned to the factory for installation via the "Return and Repair" procedure through Customer Service. For Masterpact breakers, order and install the field installable Kirk Key Interlock Provisions, S48542.For MTZ breakers, order and install field installable Kirk Key interlock provision, LV848542SP.

Kirk Single Lock Type CN22 #KC40---10 - For MTZ, Masterpact NT/NW Breakers, Powerpact P Cradles, and Powerpact P Motor Operated Breakers
Kirk Single Lock (horizontal mount) #KFL003710 add 3" roll pin - For Powerpact M, P and R Breakers
Kirk Single Lock (vertical mount) #KFL003710 - For Powerpact M and P Breakers
Kirk Double Lock (vertical mount) #KFL003720 - For Powerpact M and P Breakers
Kirk Double Lock (horizontal mount) #KFL003720 add 3" roll pin - For Powerpact R Breakers
(When the roll pin is required, be sure the Kirk part number includes the statement "add 3" roll pin".)

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings