Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a 5.0P or 5.0H trip unit be used for ground fault alarm without tripping?
Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment.

Resolution:
Yes. To have ground fault alarm without tripping, add a programmable contact module (M2C or IO), and program the trip unit for alarm.
Neither the 5.0 nor 5.0A trip units can be used because those trip units do not have the required programming functionality.
If replacing a standard trip unit (not A, P or H), the 12-pin connector for the trip unit (kit S33101 for Masterpact, S33100 for Powerpact) must also be ordered.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings