Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the suffix that designates 50 deg C calibration on the Powerpact circuit breakers?
Product Line:
Circuit Breakers

Resolution:
To meet requirements of higher ambient conditions, circuit breakers can be factory calibrated for a 50°C ambient temperature by using the CA Suffix. Circuit breakers with special thermal calibration such as CA suffix are not UL Listed. The CA suffix applies to Powerpact H, J, and Q thermal magnetic circuit breaker only.

NOTE: Electronic Powerpact breakers and Powerpact B beakers are not available with 50° calibration, however they can be applied in 50° C applications when derated properly. For more information on the electronic Powerpact H, J, L, M, P, and R frame breakers, see attached catalog pages with ambient derating tables.

Schneider Electric Australia

Attachment(s)
Rerating for Powerpact M P R.pdf [57.24 KB]
Rerating for Powerpact H J L.pdf [107.44 KB]
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings