Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU363SS, series F6? (may be shown as F06)
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the HU363SS, series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056775250 (arc suppressor not included)
-Line Base mounting screw - 4020515101 (3 required)
-Arc Suppressor Assembly - 4056635550
-Arc Suppressor mounting screw - 4020514501 (1 required)
-Lug assembly - 4025101851 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056894150 (also recommend replacing lockplate gaskets)
-Lockplate - 4056894201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screw - 2194900001 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings