Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find the part numbers for LED bulbs for 9001KM35L type LED modules?
Issue:
Where can I find the part numbers for LED bulbs for 9001KM35L type LED modules?

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony Pushbuttons 30 mm


Cause:
Product selection

Resolution:
For series J KM35L LED modules use the following numbers:
65088-052-10 Red       65088-052-11 Yellow
65088-052-12 Green    65088-052-13 Blue
65088-052-14 White

You cannot use these LED lamps in series H or earlier KM35L LED modules, as damage will result. If using Digest 172 listed bulbs in series J KM35L LED modules, they will be very dim.  Lamp part numbers are also listed on the side of the light module.
See attached

Schneider Electric Australia

Attachment(s)
Standard and Shallow Depth Light Modules.pdf [536.13 KB]
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings