Issue:
Is the 100mA fast acting fuse the correct to be used with RM17TE00?
Product Line:
Relays and Timers
Environment:
Zelio Control
Cause:
Product Features
Resolution:
Correct fuse is a 1 A fast acting CC or gG fuse on the input. There was an error in the instructions.
Is the 100mA fast acting fuse the correct to be used with RM17TE00?
Product Line:
Relays and Timers
Environment:
Zelio Control
Cause:
Product Features
Resolution:
Correct fuse is a 1 A fast acting CC or gG fuse on the input. There was an error in the instructions.
Released for: Schneider Electric Australia