Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
9013: What is the difference between M1 and M4 options?
Issue:
M1 and M4 differences

Product Line:
9013 Pressure switch

Environment:
Products sold in North America

Resolution:
The M4 form is for a Low pressure cut off, the contacts will open at 10PSI below the set cut in pressure. This is used to protect pipe from low pressure collapse in boost pump applications, and pumps running dry in low flow conditions.

The  M1 form is for a Maintained manual cut-out lever, the switch will stay off when lever is manually set in the off position. The lever will then need to be reset manually to start the operation again.  It is primarily used during extended shutdowns.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings