Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between a 9001KS52BH2 and a 9001KS53BH2?
Issue:
What is the difference between a 9001KS52BH2 and a 9001KS53BH2?

Product Line:
Selector switch

Environment:
9001K

Cause:
Product features

Resolution:
Both items are 3 position, momentary or spring return from both sides selector switches. Both
have 2 - 9001KA1 contact blocks but have different cams. The cams will determine the contact
configuration by allowing the contacts to open and close differently. Since the cams can be ordered as a repair part,
many incorrect selections can be resolved by simply replacing the incorrect cam with the the correct one.

The 9001KS52BH2 has a "B" cam and the contact configuration is as follows:
1 0 0
0 1 1
0 0 1
1 1 0

The 9001KS53BH2 has a "C" cam and the contact configuration is as follows:
1 0 0
0 0 1
1 0 0
0 0 1

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings