Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the LUCA12BL be controlled with a PLC?
Issue:
The LUCA12BL is to be controlled directly with the output of a PLC.

Product Line:
Tesys U line

Environment:
LUB32+LUCA12BL

Cause:
PLC doing remote control of the motor starter.

Resolution:
Yes, if the output of the PLC is 24 V DC and can handle an inrush of 220mA . A reversing module will add 120mA to the inrush when it has to change the direction of the motor.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings