Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where is the coil voltage or coil voltage code located on the LC1D09-D32 contactors?
Issue:
Where to find the coil voltage on the LC1D09-D32 contactors?

Product Line:
IEC Contactors

Environment:
Tesys D line contactors

Cause:
Locating the coil voltage or voltage code on a d line contactor

Resolution:
For the AC voltage, the voltage and voltage code can be found on the top of the contactor, behind the
L1 L2 and L3 terminals facing the front of the contactor, it will either be blue or white and will have
the coil voltage listed.  For example G7 120V 60/50HZ.

For DC voltage it will be listed on the front of the contactor, in the lower left corner,
next to the #14 NO screw terminal. For example: 24VDC

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings