Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Changing color caps on 9001SKR1 or 9001KR1
Issue:
Can the color caps be changed on a 9001KR1 or 9001SKR1

Product Line:
30mm momentary operators

Environment:
US product

Cause:
A Customer may wish to change the color of the cap on a momentary operator.

Resolution:
These operators are not meant to have the color cap changed.  Once a color has been inseted into the push button, it is best to replace the entire pushbutton with the new color needed.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings