Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Difference between older D2 LC1D contactors and newer LC1D contactors

Issue:
What is the difference between the older D2 style contactors where aux contacts had to be specified and the newer LC1D contactors?

Product Line:
TeSysD contactors

Environment:
US product

Cause:
Crossing into new units from old units require a review of differences

Resolution:
The older D2 style contactors required a specification of needed auxiliary contacts.  For example:

LC1D2501G6 would be an LC1D25 with 1 NC contact
LC1D2510G6 would be an LC1D25 with 1 NO contact

The newer contactors automatically come with 1 NO and 1 NC auxiliary contact.  For example:
LC1D25G7 has 1 NO and 1 NC contact

The older contactors usually had a dedicated 60hz coil.  This is designated by the 6 at the end of the part number.  The newer contactors have coils designed for 50/60hz and are signified by the 7 at the end of the part number.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings