Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
HAND-OFF-AUTO contact arrangement for 9001KS43 or 9001SKS43
Issue:
What contacts are needed for a standard HAND/OFF/AUTO (HOA) arrangement on a 9001KS43 or 9001SKS43 selector switch?

Product Line:
9001SK/9001K selector switches

Environment:
US Product

Cause:
Selector switches sometimes need contacts added in the field.

Resolution:
For a traditional HAND/OFF/AUTO selector switch function wherein one contact is closed only in the left hand position, no contacts are closed in the middle position, and a second independent contact is closed only in the right hand position, use a 9001KA1 contact block on the back of the 9001KS43/9001SKS43 selector switch.  With this particular switch (which uses a C cam), the NC contact will be closed only in the left hand position (HAND), the NO contact will be closed only in the right hand position (AUTO), and no contacts will be closed in the middle position (OFF).

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings