How can we help you today?

What is the replacement lens cap for a ZB4 or ZB5 BA9 (incandescent) illuminated push button with extended push?

Issue:
What is the replacement lens cap for a ZB4 or ZB5 BA9 (incandescent) illuminated push button with extended push?

Product Line:
22mm Illuminated Push Buttons

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:

White: ZBV931

Green: ZBV933

Red: ZBV934

Yellow: ZBV935

Blue: ZBV936

Clear: ZBV937

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings