Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Trace SW turns the generator on but then it turns off right away.
Trace SW Inverter/Charger is not controlling the generator correctly

Problem: The Generator start relays are not turning on and off the generator properly
Solution: Determinewhether generator has 2-wire or 3-wire start configuration.
Ex.(1) If the generator is 2-wire, meaning it starts and runs when wires are connected and shuts off when the wires are disconnected (from each other),  set to Run.
RY7 Common and RY7 N.O. (Normally Open) contacts remain closed while generator is running.
Ex.(2) If the generator is 3-wire, set to Glowstop, then RY7 remains open while the generator is running. RY8 is used for cranking.
Refer to relay timing chart on pg.78 of attached manual.
When the SW loses DC power, the mode goes back to Run by default.

Schneider Electric Australia

Attachment(s)
SWSeriesOwnersMan.pdf [2.58 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales inquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings