Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to enable or disable an ION Meter Web Page?

Issue
When trying to connect to an ION meter through a web browser, an error " Page can not be displayed" or "This site can't be reached", depending on which web browser, is displayed.

Product Line

ION 8650, 8600, 7650, 7550, 7600, 7500
PM8000


Environment

ION Meter Web Page

Cause
The ION Meter Web Page has been disabled.

Resolution
Enable the ION Meters Web Page functionality.
Note: For PM8000 meters, ION Setup V3.0.15140.02 or later must be used. The latest version of ION Setup can be obtained from FA212816.

1. Connect to the meter in Advanced Mode using ION Setup.
2. Select the Comm Modules folder and then the Ethernet module.
3. Under the Setup Registers Tab, select ETH1 Enable Webserver and change the value to 'Yes' to enable the Web server, or 'No' to disable it. (Refer to the screen shot below)

IONsetup

NOTE: the ETH1 Webserver Config Access will enable or disable the ability to make configuration changes from the ION Meter Web Page.

Note: For instructions on connecting to an ION Meter in Advanced Mode, please refer to ION Setup 3.0 User Guide. Latest ION Setup User Guide can be obtained by visiting following link:
https://www.se.com/ww/en/product-range-download/61461-ion-setup-3.0

Please note that if the device is communicating over a managed switch, you may need to use the IP address signed by the switch when trying to browse the meter webpage.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings