Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use an ATS48 type starter to supply a slip-ring motor?

The ATS48 could be used with Slip Ring motor, but due to the fact a Slip Ring motor is designed for high torque applications the most efficient answer would be to use an ATV71 / ATV930 / ATV950 constant torque variable speed drive as using the soft start on this application would reduce the available torque on start up due to the ramped voltage.

If a Soft Start Unit is to be used to start a Slip Ring Motor there are a number of things to be considered.

The resistors are to be removed and the Rotor shorted out, but engineers agree that a small amount of resistance should be maintained.  This is usually achieved in the cables.

This has in theory turned the motor into a Squirrel cage motor with HIGH TORQUE starting.  To use a soft start on a high torque application the current limit must be set to maximum this would mean the motor would be able to pull high current to get it away.  The average starting current for a Slip Ring Motor is 250% of its Full Load Current where as if using a Soft Start it would be 700% of Full Load Current.  Using a 55Kw motor as an example at 400V

SLIP RING

FLC x 250 =      100 x 2.5 = 250A

SOFT START

FLC x 700 =      100 x 7 = 700A

As can be seen from the above calculations all the wiring and circuit equipment will have to be changed to be able to cope with the higher currents

So as previously stated the best option if you are replacing a Slip Ring Starter is to use an Altivar Variable Speed Drive from the ATV71 / ATV930 / ATV950 range





Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings