Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to disassemble an XB4 Operator
Issue:
How do you disassemble an XB4 operator and mounting collar

Product Line:
XB4 line of products, Harmony 22mm

Environment:
US Products

Resolution:
See attached file for representation.
To disassemble an XB4 operator you need to pull the button/selector switch out of the mounting collar by using a small flat screw driver to pull down on the metal "L" shaped part on the bottom of the mounting body. You can then remove the contacts using the flat screwdriver to lift on the metal hooks that hold the contact block to the back of the mounting collar.

To assemble you snap the head into the mounting body by lining up the arrow on the collar with with arrow on the head. You can add contact blocks by pushing the bottom latch of the contact into the collar, and then you push the contact to the collar so that the metal hooks latch on to the back of the collar.

Schneider Electric Australia

Attachment(s)
XB4 XB5 instructions.pdf [293.71 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings