Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why are there 2 coils for LC1F1700?
Issue:
Why does the LC1F1700 use two coils

Product Line:
IEC Contactors - GIC Product

Environment:
US Product

Cause:
Product specifications

Resolution:
Two coils are used to balance the device as it is too long for a single coil.  Both coils are wired in series at roughly half (or slightly less) of the control voltage used so that the voltage is split evenly between the two coils.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings