Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Why do CSEDs (RC & QC devices) with factory installed tunnel kits allow the service wires to be exposed at the bottom of the device?
Issue:
Adjusting CSED factory installed tunnel kit following completed utility wiring.

Product Line:
Combination Service Entrance Devices

Resolution:
The Specific CSED that contain the tunnel kit will be shipped from the factory, with the tunnel in a raised position. This allows the installer to pull the Service Wires up from the bottom endwall and through the tunnel area when underground feeding the device. The tunnel contains an adjustment screw so it can be raised or lowered once the Service Wires are in place.

Once the Service Wires are installed, the adjustment screw should be loosened or removed and the tunnel moved down, allowing the hasp on the tunnel, to go through the bottom endwall. This will allow the Utility company to lock and seal the tunnel, preventing any unauthorized access of the Utility Service Wires. The tunnel covers the whole left side of the load center gutter area of the CSED, and once the tunnel is down and locked, tighten or reinstall adjustment screw.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings