Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for a 20A 10mA RCBO?

The part number for a 20A 10mA RCBO is A9D10820 or  4RCBE220/10S
A9D10820 will fit
Schneider chassis but cannot not be used for hospitals or body protected areas as it does not switch neutral.
The Clipsal 4RCBE220/10S is suitable for hospitals but will not fit to Schneider chassis.

A9D10820 Product picture4RCBE220/10S
A9D10820 iC60H - earth leakage circuit breaker
1P + N - C curve - 20 A - 10 mA - 240 V
4RCBE220/10S SLIM CLIPSAL
20A 10mA A-TYPE 6KA


For more information see :
http://eshop.schneider-electric.com/product.aspx?org=21&lang=1&dist=276&prod_id=A9D10820
http://www.clipsal.com/Trade/Products/ProductDetail?catno=4RCBE220/10S

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings