Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Citect - Displaying multiple screens on one monitor

Applies To: Citect SCADA All Version

Summary:  Previously I had multiple monitors displayed in an array, however now I want to use one large display and have multiple Citect windows displayed on it.

Solution:  Remove any MultiMonitor parameters from the Citect.ini (Computer Setup Editor). On startup call a Cicode function to open multiple windows using the WinNewAt Cicode function as follows. This is done in the Computer Setup Wizard, on the Startup Function Setup menu. In this case the dimensions of each page is exactly a quarter of my screen resolution (1920x1080). I then offset where the page is displayed using the X and Y coordinates of the WinNewAt function call.

WinNewAt("test1",0,0,2);
WinNewAt("test2",960,0,2);
WinNewAt("test3",0,540,2);
WinNewAt("test4",960,540,2);

Keywords:  monitor, display, multi monitors, display, pages

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales inquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings