Search FAQs
Osisense XC - What is the UL94 flame classification of the blue XCMW102 plastic case?
The plastic case of the blue XCMW102 wireless & batteryless limit switches is a blue Valox 553, or PBT+PC GF30. It is flame classified UL94 V-0. PBT stands for polybutylene terephthalate, PC for polycarbonate, GF30 means 30% glass fiber reinforced
Released for:Schneider Electric Australia
Attachment(s)
Explore more