{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Why does Control Expert v14.0 STU save take so long?

Issue
There is a lot of latency in the handling of the STU file with Control Expert v14.0

Product line
EcoStruxure Control Expert

Resolution
This was an issue when using version 14.0 which was addressed with the HF0556733R hot fix.

Hot Fix is attached.

Schneider Electric Australia

Attachment(s)

ControlExpert_V140_HF0556733R.zipControlExpert_V140_HF0556733R.zip [627.48 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: