Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the XENL1121 and XENL1111?
Issue:
What is meant by base mount contacts like the XENL1111 used in a XALB control station?

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony Pushbuttons

Cause:
Obsolete Product's Features

Resolution:
They are base mounted contacts for use in the XALB control stations.  They mount in the back of the enclosure instead of to the back of the operator. This make wiring easier.
The XENL1111 is a normally open contact and the XENL1121 is a normally closed.

Schneider Electric Australia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings