Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What type of LED's can be used on C-Bus Dimmers?

Firstly you will need to confirm whether your C-Bus system contains C-Bus Leading Edge Dimmers or C-Bus Universal Dimmers, You may need to consult with your EcoXpert in Light and Room Control which one(s) you have if unsure.

The general recommendations for LED compatibility with C-Bus Dimmers is as follows
1) Ensure your LED's have a dedicated LED Driver (electronic transformer) that supports your C-Bus Dimmer type
2) Bench test that the LED Driver is of good quality and works as expected at your site
3) C-Bus Dimmer channels require >25W of load if less is connected to a specific channel that channel will require the addition of a 31LCDA (Load Corrective Device)

C-Bus

4) If the dimming range of the LED fittings is specified by the manufacturer - the installer can programmer the Min/Max settings of the C-Bus Dimming channel to match the LED fittings dimming range.

Note:
C-Bus Leading Edge Dimmers will require LED's which have electronic transformers (LED Driver) which support Leading Edge AC phase control dimming (as noted in the compatible loads section of the installation manual)

C-Bus


C-Bus Universal Dimmers will require LED's which have electronic transformers (LED Driver) which supports Trailing Edge AC phase control dimming (as noted in the compatible loads section of the installation manual).
Although Universal Dimmers can support leading OR trailing edge AC phase control dimming it needs to be exclusively one or the other (NOT BOTH). As such LED Drivers which note LE/TE LED Driver are NOT suitable for the Universal Dimmer.

C-Bus
IMPORTANT: Clipsal by Schneider Electric & Schneider Electric DO NOT make LED's which are compatible with C-Bus NOR can we recommend specific LED Drivers for your C-Bus Dimmer type as LED Dimming and Driver technology is continually changing. The above is a guideline to assist you choose a compatible LED with dedicated LED Driver that supports your dimmer in question. As noted above please have your EcoXpert in Light and Room Control bench test LED Fittings and LED Driver for suitability on your C-Bus Network.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings