Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the available methods for M580 ModbusTCP/IP communication to a Modbus slave/server?
Method 1 is IO scanning which can be set up through the DTM browser of Control Expert. The created Modbus variables will appear in the Device DDT Variables table.

Method 2 is explicit messaging which involves using Read_var, Write_var and/or Data_Exch function blocks in the program. Note Read_Var and Write_Var must be used in combination with the ADDM or ADDMX function block.


IO scanning (implicit messaging) can be done at the same time as Read_var and Write_var (explicit msg) to the same modbus slave and to the same registers. These can also be done simultaneously to different registers.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings