Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to properly select location and mounting of daligateway2 (5502CDGP230)

The C-Bus DALI-2 Gateway is designed to be installed in a distribution cabinet, mounted on a DIN rail (type DIN EN60715), in a horizontal position.

There should be adequate ventilation to prevent overheating of this unit, this can be achieved by using larger distribution boards as opposed to small domestic distribution boards.

C-Bus Cat-5e cables Should be adequately separated or segregated as defined in local wiring regulations.

Note: Use the heat load value of all the units in the cabinet to select a cabinet with correct ventilation. Ensure that the temperature around the unit is less than 45C.

Schneider Electric Australia

Attachment(s)
pha5979201_asm_ISO.png [4.45 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings