Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use the 2P iC60 (N or H) MCB for 400V application (e.g. measuring 400V across phase to Neutral)?
Issue:

Can use the 2P iC60 (N or H) MCB for 400V application measuring 400V across phase to Neutral?

Product Line:

Acti 9

Environment:

iC60 (N or H)

Resolution:

Yes, MCBs Acti9 iC60N/H 2P can be used under Ue (Ph/N) or (Ph/Ph)=400Vac applications.
You can refer to breaking capacities declared in catalogue pages for Ue=380-415Vac (e.g Icu=10kA for iC60N 2P C 40A including ref.A9F44240).

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings