Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I confirm that we can achieve earth fault alarm without an external sensor in 3PH4W MTZ2 20H1 – Micrologic 5.0X?
Issue:

Can we achieve earth fault alarm without an external sensor in 3PH4W

Product Line:

Circuit Breakers

Environment:

Masterpact MTZ, Micrologic X control unit

Resolution:

As per MasterPact MTZ - MicroLogic X Control Unit User Guide, the ground -fault current is calculated or measured as below

MasterPact MTZ - MicroLogic X Control Unit User Guide Link:

https://www.se.com/au/en/download/document/DOCA0102EN/


Ground Fault Current Calculating

The basic principle of ground fault current Ig is the vectorial sum= I1+I2+I3+In.
Please see below one example for better understanding:
1.      If customer is 3phase 4 wire system (with Neutral), there are two solutions of ground fault alarm/protection:
1)     Customer can select 3P breaker, but breaker should be configurated as 3P+ENCT, that means the external neutral CT sensor is necessary.
2)     Customer can select 4P breaker, no necessary for external neutral CT sensor.

2.      If customer is 3phase 3 wire system (without Neutral):
Customer should select 3P breaker and declares the ENCT to “NO”, no necessary for external neutral CT sensor.
Anyway, if there is neutral phase in customer system, neutral current should be measured in 4P or 3P with external sensor.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings