How can we help you today?

Harmony IPC Low Memory Error

From the Task Manager, check the memory usage of each application. If there is an application with excessive usage, try to close it.

  1. Go to Control Panel->View advanced system settings (you can just type it from the Start bar).

task bat manager

  1. Then in the System Properties dialog, go to the Advanced Tab.
  2. Under Performance, click on the Settings… button.
  3. In Performance Options dialog, go to the Advanced Tab.
  4. Under Virtual Memory, click on the Change… button.
  5. In the Virtual Memory dialog, select "Custom Size" settings at 4GB(= 4096MB) or 6GB(=6144MB).
  6. Click OK.

instruction

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings