Where to download the C-Bus Toolkit 1.17.1?
Release Date: 08/12/2023
Version: V1.17.1
Reference: C-Bus_Toolkit_V1.17.1
C-Gate: 3.2.2 (build 1716)
Operating systems: Windows 11 Professional (64-bit), Windows 10 Professional (64-bit), Windows 10 Enterprise (64-bit), Windows 10, Windows 8, Windows 7.
Bug fix:
Updates to C-Gate 3.2.2 include:
Link to download C-Bus Toolkit 1.17.1
https://www.se.com/au/en/download/document/C-Bus-Toolkit_V1.17.1/
Release Date: 08/12/2023
Version: V1.17.1
Reference: C-Bus_Toolkit_V1.17.1
C-Gate: 3.2.2 (build 1716)
Operating systems: Windows 11 Professional (64-bit), Windows 10 Professional (64-bit), Windows 10 Enterprise (64-bit), Windows 10, Windows 8, Windows 7.
Bug fix:
- Issue resolved when clicking the ‘+’ button to add a new application in the eDLT unit dialog.
Updates to C-Gate 3.2.2 include:
- Update C-Bus DALI-2 Gateway firmware version default to version 1.7.0.
- Device update to support C-Bus DALI-2 Gateway and DALI Device Primary Control Function.
- Added support for C-Bus Network Devices section firmware update notification.
- Fixed the transfer of new levels to a C-Bus Controller within existing groups.
Link to download C-Bus Toolkit 1.17.1
https://www.se.com/au/en/download/document/C-Bus-Toolkit_V1.17.1/