Where to download the SpaceLogic C-Bus Commission V2.0.0?
Where to download the SpaceLogic C-Bus Commission V2.0.0?
Release Date: 26/10/2023
Version: V2.0.0
Reference: C-Bus-Commission_V2.0.0
C-Gate: 3.2.0 (build 1674)
Operating systems: Windows 11 Professional (64-bit), Windows 10 Professional (64-bit), Windows 10 Enterprise (64-bit), Windows 10.
First Release:
The new C-Bus Commission software is built upon and includes a new version of C-Gate (C-Gate 3.2.0). The new version of C-Gate requires that updates are performed to the broader suite of C-Bus software installed on the PC including C-Bus Toolkit, plus other applications such as PICED, HomeGate, etc.
If you have C-Bus Toolkit V1.16.x or earlier currently installed on your PC, you must also install the latest release of C-Bus Toolkit (V1.17.0 or later) accompanying this release of C-Bus Commission. Both C-Bus Toolkit and C-Bus Commission software applications are bundled with C-Gate 3.2.0.
The new C-Bus Commission software offers capabilities to design a C-Bus project and incorporate the new C-Bus DALI-2 Gateway and DALI devices as well as the new C-Bus Digital Dimmer devices.
Important Notes:
This release includes support for the new project file format used by C-Gate 3.2.0. Only projects that have been successfully converted can be opened.
Once projects have been converted to the new format, they cannot be used by C-Gate 2 or below.
We strongly recommend creating a separate back up of projects before installing and running this release.
Link to download the SpaceLogic C-Bus Commission V2.0.0
https://www.se.com/au/en/download/document/C-Bus-Commission_V2.0.0/
Release Date: 26/10/2023
Version: V2.0.0
Reference: C-Bus-Commission_V2.0.0
C-Gate: 3.2.0 (build 1674)
Operating systems: Windows 11 Professional (64-bit), Windows 10 Professional (64-bit), Windows 10 Enterprise (64-bit), Windows 10.
First Release:
The new C-Bus Commission software is built upon and includes a new version of C-Gate (C-Gate 3.2.0). The new version of C-Gate requires that updates are performed to the broader suite of C-Bus software installed on the PC including C-Bus Toolkit, plus other applications such as PICED, HomeGate, etc.
If you have C-Bus Toolkit V1.16.x or earlier currently installed on your PC, you must also install the latest release of C-Bus Toolkit (V1.17.0 or later) accompanying this release of C-Bus Commission. Both C-Bus Toolkit and C-Bus Commission software applications are bundled with C-Gate 3.2.0.
The new C-Bus Commission software offers capabilities to design a C-Bus project and incorporate the new C-Bus DALI-2 Gateway and DALI devices as well as the new C-Bus Digital Dimmer devices.
Important Notes:
This release includes support for the new project file format used by C-Gate 3.2.0. Only projects that have been successfully converted can be opened.
Once projects have been converted to the new format, they cannot be used by C-Gate 2 or below.
We strongly recommend creating a separate back up of projects before installing and running this release.
Link to download the SpaceLogic C-Bus Commission V2.0.0
https://www.se.com/au/en/download/document/C-Bus-Commission_V2.0.0/
Released for: Schneider Electric Australia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.