Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to troubleshoot C-Bus Automation Controller LUA Scripts
C-Bus Application and Network Automation Controllers utilize LUA scripting to provide an additional level of customizable functionality via LUA event-based, resident or scheduled LUA scripting. The following troubleshooting tips can assist in troubleshooting LUA script issues.

Save Script - Syntax errors are shown when saving the script
These errors relate to general LUA command/statement syntax

example 1: in following if - then - else - end condition the following LUA script is missing the closing "end" statement

if (StrRmReedSwitch == false) then
-- Turn ON the Store Room Alarm and Alarm Light
SetCBusState(0, 56, 77, true)
SetCBusState(0, 56, 79, true)
else
SetCBusState(0, 56, 77, false)
SetCBusState(0, 56, 79, false)

results in the following error when attempting to save

LUA Syntax Error

Show Error Logs - Logical errors are shown when "Error log" is selected (1), and from the Error log window selecting "Show errors only for current script" (2) and "Clear" (3) then running the LUA script - by changing related object statuses etc in Object Tab, Visualization or Run Script

Logic errors relate to logical issues with the LUA Script such as trying to retrieve the state of an uninitialized group or trying to retrieve the state of a group that does not exist, or performing incompatible arithmetic etc.

Show error log

example 2: Library cbuslogic:0: unable to find 0/56/250 --- (check if application 56, group address 250 object exists?)
example 3: Library cbuslogic:0: unable to decode 0/56/150 --- (check if application 56, group address 150 object currently nil "un-initialized")
example 4: User script:5: attempt to perform arithmetic on global 'StmRmTempSwitch' (a nil value) stack traceback: --- (check compatibility of arithmetic)

The following LUA script tries to perform a mathematical addition of a boolean returned from GetCBusState and an integer value resulting in Error log message

-- Get state of Store Room - Reed Switch on the local network
StmRmTempSwitch = GetCBusState(0, 56, 78)
IntValue = 5
CalcValue = IntValue + StmRmTempSwtich

Log messages which can help further troubleshoot LUA script issues are shown when "Log" is selected (1), and from the Current logs window selecting "Show logs only for current script" (2) and "Clear" (3) then running the LUA script - by changing related object statuses etc in Object Tab, Visualization or Run Script

Log messages can be used to log values of c-bus states, levels, variables and determine whether expected conditional and behavior is being met or may provide answer why a condition is not met and a certain block of the LUA script is not being executed.

example 5: Running the following script shown in image and turning the Strong Room Reed Switch group OFF and ON shows script is working as expected.

LUA Script Current logs

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings