Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is their no display on the VIP400 relay

Please note, the VIP400 is a stand alone protection relay powered by its current sensors - when current is present in the MV network, the protections and the display work and it is possible to enter settings and view measurements - the VIP operates at a pickup current value as mentioned in the table below.

Pickup Curent

When no current is flowing through the circuit breaker or when the current is too low, the VIP is off and nothing appears on its display. If current appears, the protection functions are activated and trip the circuit breaker or not, according to the settings. The additional time for the VIP relay to start when current appears is called the pick up time and is mentioned in the table below.

VIP400

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings