Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME Upgrade/Install fails at the "Create Databases" step due to a "FK_Alarm_PQEventID" error

Issue

User is unable to install or upgrade because of an "FK_Alarm_PQEventID" error at the "Create Databases" step.

Upon investigating the ION_Data.log you see the following: "The DELETE statement conflicted with the REFERENCE constraint "FK_Alarm_PQEventID". The conflict occurred in database "ION_Data", table "dbo.Alarm", column 'PQEventID'."

Product

EcoStruxure Power Monitoring Expert

Resolution

*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

---------------------------------------

Script:

USE [ION_Data]

GO

ALTER TABLE [dbo].[Alarm] DROP CONSTRAINT [FK_Alarm_PQEventID]

GO

ALTER TABLE [dbo].[Alarm] WITH NOCHECK ADD CONSTRAINT [FK_Alarm_PQEventID] FOREIGN KEY([PQEventID]) REFERENCES [dbo].[PQ_Events] ([EventId])

GO

ALTER TABLE [dbo].[Alarm] CHECK CONSTRAINT [FK_Alarm_PQEventID]

GO

---------------------------------------

After you apply the script you can attempt the install/upgrade again.

Schneider Electric Australia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings