Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to fix a usb cable driver crash issue on Zelio smart relay after Windows update

Zelio Cable Drive Installation Steps Sometimes after an Windows update, drivers for cable will crash, then it is unable to connect Zelio relay with PC. To fix this issue, please follow below step and use the picture for reference.

Step 1: Make sure the SR2 USB01 cable is connected to PC. In windows, go to Control Panel and then find Device Manager. Find Ports (COM & LPT) and then find Zelio Serial Port.

Step 2.1: Double click Zelio Serial Port. to open the property window, move to Driver tab, then click Uninstall Device. In the popup window, tick Attempt to remove the driver from this device, then click Uninstall.

Step 2.2: In the Device Manager, find Universal Serial Bus controllers and then  find Zelio SR2 USB01 H2.x. double click it to open the property window, move to Driver tab, then click Uninstall Device. In the popup window, tick Attempt to remove the driver from this device, then click Uninstall.

Step 3: Reinstall the driver by using SR2_USB01_H2.x_Setup.exe.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings