Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Upgrade a BMENOC03x01.3 to BMENOC0301.4 in an existing application

Issue:

How to change the BMENOC03x1.3 to BMENOC03x1.4 in an existing application , after the firmware off the NOC Module

has been updated to latest firmware

Product Line:

BMENOC03x1

Resolution:

Please follow the below steps ,

1.Please Export the project file to .ZEF then from search bar please open the M580 Application Update

Image_1

2. Please update the Converter Section from BME NOC DIO 3x1 from version .3 to version .4

Image_2

3. Finally , please upload the project file that needs to converted and Click Next and file will be converted with BMENOC03x1.4

NOTE:

The Scope of this tool will be to update M580 Application with a CPU version Starting from SV 02.30

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings